Technical FAQs

Ask a Question

What are the causes a Wrench 1 to be displayed on a Sepam relay.

There could be below five reasons that will cause a wrench 1 to be displayed on the Sepam relay:
1. CCA6xx is not connected to the relay
2. The relay is configured for an MES (I/O) module and it is not connected
3. A cable is connected to the communications port on the relay and the relay is not configured for an ACExxx module.
4. The terminal strips are not connected to the relay.
5. Major internal fault in the relay.
Was this helpful?
What can we do to improve the information ?