Technical FAQs

Ask a Question

With the capacitor duty contactor can we use a MPCB for short circuit.

It is possible to protect a capacitor bank with circuit breakers.
Their sizes should be select taking a coefficient of 1.5 times the nominal current of the capacitor (due to tolerances).
Was this helpful?
What can we do to improve the information ?