Technical FAQs

Ask a Question

How to send command to control the digital output using Modbus protocol to PM5350.

For PM5350 meter, to energize Digital output, you should use command code 6003; to de-energize digital
output, you should use command code 6002.
 
Here is an example for writing register to "De-energize Digital Output DO2" via using Modbus tester (or PMC Modbus).
Select Data Type: W16 (to write Multiple registers);
Select Starting Register: 5250;
Select # of Resister: 3;
Write: 405250 ->6002; 405251 ->0; 405252->2
Press "Write" button.
 
Please keep in mind that the command write must be done in a block write and it will not work if you write each register individually!
Was this helpful?
What can we do to improve the information ?