Technical FAQs

Ask a Question

How can we change the User Access Permission in Vijeo Citect which is authorized to acknowledge the alarms.

To modify the privilege level to acknowledge the alarms you need to set the following INI parameter in Citect INI files.
Which determines the privilege level a user requires acknowledging alarms. Permissible value for this parameter is 0 to 8 and the default value is 1.
After that user which is having the privilege level greater than specified in above parameter is only authorized to acknowledge the alarms.
Was this helpful?
What can we do to improve the information ?