Technical FAQs

Ask a Question

Can we use other loopback addresses in Vijeo Citect SCADA in addition to 127.0.0.1.

All the Internet Protocol address from any address in the range 127.0.0.1 to 127.255.255.254 is mapped as loopback ip address.
Loopback address is designated for the software loopback interface of a machine. The loopback interface has no hardware
associated with it, and it is not physically connected to a network.
 
However, by design, Citect uses the most commonly-used loopback address only, which is 127.0.0.1. When using any other
addresses, Citect will not recognize this IP address and you will not be able to set this computer as a server in the computer
set-up wizard, and will receive #coms when the project is run.
Was this helpful?
What can we do to improve the information ?