Technical FAQs

Ask a Question

How can we set PC time from Vijeo Citect when we do not want operator to minimize the Citect runtime to access windows.

If you do not want the operator to access window and want PC system time to be set from Vijeo Citect Runtime
then you can use the following function:
 
TimeSet(Time)
Where
Time:
The time/date variable to which the new time is set. Sets the time on the computer from where it is being launched.
 
For example you can use this function as follows:
! set the time to 11:43 on June 23 1993
time = StrToTime("11:43:00") + StrToDate("23/6/93");
TimeSet(time);
Was this helpful?
What can we do to improve the information ?