Technical FAQs

Ask a Question

Why is the Download selection in Vijeo Designer grayed out.

The download option is grayed out in Vijeo Designer only when the Vijeo Designer trial version is installed.
 
You can only download into the HMI either in Vijeo Designer unregistered or licensed.
But please take note that with unregistered version you cannot use full features of Vijeo Designer
also you can not add additional targets in Vijeo Desginer.
Was this helpful?
What can we do to improve the information ?