Technical FAQs

Ask a Question

How to select the license point counts for Vijeo Historian.

The historian license is based on the amount of data being stored. (VJHNS2110xx). The number of points is the maximum number
 of tags and trends being historized and stored in the system (the number of alarms stored is unlimited).
For example for VJHNS211011 150 tags stored
Purchases of Vijeo Historian will now include 1 Historian User/Device CAL (Client Access license) which determines how many user
or device can access the historized data from historian.
Was this helpful?
What can we do to improve the information ?