Technical FAQs

Ask a Question

Can we create template for the panel in Vijeo Designer.

Yes, the templates for the panel in Vijeo Designer can be created. All the panel that has been created under Master Panels
section is being used as template for other base panels.
 
To include the Template (Master Panels) into base panel go to Base Panels properties, under Master Panels select the Master
Panel you want to use as template for this base panel.
Was this helpful?
What can we do to improve the information ?