Technical FAQs

Ask a Question

Is it possible to use the Quantum HSBY processor 140CPU67160 with RIO ( S908) and Quantum Ethernet IO ( QEIO ) together.

This CPU 140CPU67260 and 140CPU67261 supports the mix between S908 and QEIO.
This will allow customer that have an existing application with the 140CPU67160 + S908 and want to extend with QEIO.
Indeed the 140CPU67160 doesn’t support the mix of S908 + QEIO. The customer will be able to replace the existing CPU
by the new one to get this additional feature without having to change his Fiber optic type on the HSBY inter-link.
Was this helpful?
What can we do to improve the information ?