Technical FAQs

Ask a Question

What accessory is needed to connect the two reels of RG11 trunk cable.

Ground Blocks is to be used while connecting two reels of RG11 trunk cable.
60-0545-000 Ground Block consists of two female in-line F connectors and a separate screw hole
binding for attaching a ground wire. The grounding block has two mounting holes, allowing it to be mounted
to a flat surface. Ground blocks have a low insertion loss, and they usually are not figured into the attenuation
calculations unless five and has an impedance of 75 ohms.

Was this helpful?
What can we do to improve the information ?