Technical FAQs

Ask a Question

Is it possible to install EasyPact CVS MCCB in class II switchboards.

All EasyPact CVS circuit breakers are class II front face devices. They can be installed through the door of class II
switchboards (as per IEC standards 61140 and 60664-1) without downgrading switchboard insulation.
Installation requires no special operations, even when the circuit breaker is equipped with a rotary handle.
Was this helpful?
What can we do to improve the information ?