Technical FAQs

Ask a Question

What is the degree of protection for EasyPact CVS circuit breakers.

The following indications are in accordance with standards IEC 60529 (IP degree of protection) and
IEC 62262 (IK protection against external mechanical impacts)for EasyPact CVS circuit breakers.
 
Bare circuit breaker:
  •  with toggle: IP40, IK07 front face
  •  with extended rotary handle: IP 55, IK08
 
Circuit breaker installed in a switchboard:
  • with toggle: IP40, IK07 front face
  • with extended rotary handle: IP 55, IK08
 
Was this helpful?
What can we do to improve the information ?