Technical FAQs

Ask a Question

What are the international standards to which EasyPact circuit breakers are in compliance for Climatic withstand tests .

The EasyPact CVS circuit breakers are in compliance with the tests defined by the following standards for
extreme atmospheric conditions:
 
  •  IEC 60068-2-1: dry cold (-55°C)
  •  IEC 60068-2-2: dry heat (+85°C)
  •  IEC 60068-2-30: damp heat (95 % relative humidity at 55°C)
  •  IEC 60068-2-52 severity level 2: salt mist.
 
Was this helpful?
What can we do to improve the information ?