Technical FAQs

Ask a Question

How many electrical auxiliaries can we accommodate in EasyPact CVS circuit breakers.

The number of electrical auxiliaries which can be accommodated in EasyPact Circuit breakers are given below
 
EasyPact CVS100/160/250
 
 5 indication contacts
Ø  2 ON/OFF (OF1 and OF2)
Ø  1 trip indication (SD)
Ø  1 fault-trip indication (SDE)
Ø  1 earth-fault indication (SDV), when the device is equipped with  a Vigi module.
 
1 remote-tripping release
Ø either 1 MN undervoltage release
Ø or 1 MX shunt release.
 
EasyPact CVS400/630
 
6 indication contacts
Ø 3 ON/OFF (OF3)
Ø 1 trip indication (SD)
Ø 1 fault-trip indication (SDE)
Ø 1 earth-fault indication (SDV), when the device is equipped with a Vigi module.
 
1 remote-tripping release
Ø either 1 MN undervoltage release
Ø or 1 MX shunt release.
 
All these auxiliaries can be installed with a rotary handle.
The illustration shown (TMD, MA, NA and ETS 2.3 standard) indicates auxiliary possibilities depending on the type of trip unit.
 
Was this helpful?
What can we do to improve the information ?