Technical FAQs

Ask a Question

Is there any test equipment available to test ETS electronic trip units of EasyPact CVS circuit breakers.

The Test equipment available to test ETS electronic trip units of EasyPact CVS circuit breakers are given below.

Mini test kit
The mini test kit is a portable unit requiring no external power supply, used to check operation of the electronic trip
unit and circuit breaker tripping.
It connects to the test connector on the front of the circuit breaker.
Required power source: five 9 V alkaline batteries (not supplied).



 
Portable test kit
The portable test kit is used to check all aspects of the protection functions:
  • long time protection
  • short time protection
  • instantaneous protection
  • earth-fault protection.
Required power source: 110 or 220 V AC, 50/60 Hz.
 
Spare test plug and wiring kit
A spare test plug and wiring kit are available for this offer.


Was this helpful?
What can we do to improve the information ?