Technical FAQs

Ask a Question

Can the standard and the extended rotary handles of EasyPact CVS circuit breakers be padlocked.

In standard situation the EasyPact CVS circuit breakers rotary handles (standard or extended)can be padlocked  
in the OFF position, using 1 to 3 padlocks, shackle diameter 5 to 8 mm.
Was this helpful?
What can we do to improve the information ?