Technical FAQs

Ask a Question

What is the Utilisation category of EasyPact CVS circuit breakers.

The Utilisation category of EasyPact CVS circuit breakers is “A”.
The standard IEC 60947-2 defines two utilisation categories, A and B, depending on breaker discrimination with
upstream breakers under short-circuit conditions.
1-Category A - Circuit breakers not specifically designed for discrimination applications.
2-Category B - Circuit breakers specifically designed for discrimination, which requires a short
time-delay (which may be adjustable) and a rated short-time withstand current in compliance with the standard.
Was this helpful?
What can we do to improve the information ?