Technical FAQs

Ask a Question

Is it possible to add a Vigi module on EasyPact CVS Circuit breakers to provide an add-on protection against insulation faults.

It possible to add a Vigi module on EasyPact CVS Circuit breakers to provide an add-on protection against insulation faults.
 
A Vigi module can be added to any three or four-pole EasyPact CVS100 to 630 circuit breaker to form a Vigi CVS.
 
Please refer the below Vigi module selection

Was this helpful?
What can we do to improve the information ?