Technical FAQs

Ask a Question

Are the EasyPact CVS circuit breakers in compliance to the tests for electromagnetic or mechanical vibrations.

EasyPact CVS devices resist electromagnetic or mechanical vibrations.
Tests are carried out in compliance with standard IEC 60068-2-6 for the levels required by merchant-marine
inspection organisations (Veritas, Lloyds, etc.)
  •  2 to 13.2 Hz: amplitude ±1 mm
  • 13.2 to 100 Hz: constant acceleration 0.7 g. 
Excessive vibration may cause tripping, breaks in connections or damage to mechanical parts.
Was this helpful?
What can we do to improve the information ?