Technical FAQs

Ask a Question

What is the Utilisation category of EasyPact MVS circuit breakers.

The Utilisation category of EasyPact MVS circuit breakers is ‘B’.
 
The standard IEC 60947-2 defines two utilisation categories, A and B, depending on breaker discrimination with upstream breakers under short-circuit conditions.
  • Category A - Circuit breakers not specifically designed for discrimination applications.
  • Category B - Circuit breakers specifically designed for discrimination, which requires a
    short time-delay (which may be adjustable) and a rated short-time withstand current
    in compliance with the standard.
 
Was this helpful?
What can we do to improve the information ?