Technical FAQs

Ask a Question

What is the maximum operational voltage Ue at which EasyPact MVS circuit breakers can be operated.

The maximum operational voltage Ue at which EasyPact MVS circuit breakers can be operated is 690V AC , 50/60 Hz.
Was this helpful?
What can we do to improve the information ?