Technical FAQs

Ask a Question

What is the Breaking capacity of the EasyPact MVS circuit breakers.

The Breaking capacity of EasyPact MVS circuit breakers is available as Type ‘N’ and Type ‘H’ for different
rated operational voltages i.e. 440 V AC and 690 V AC.
Please refer the below chart
Was this helpful?
What can we do to improve the information ?