Technical FAQs

Ask a Question

What is the Impulse withstand voltage and rated insulation voltage of Easypact MVS circuit breakers.

The Impulse withstand voltage ‘Uimp’ and rated insulation voltage ‘Ui’ of Easypact MVS circuit breakers
 are 12 kV and 1000 V respectively.
 
Was this helpful?
What can we do to improve the information ?