Technical FAQs

Ask a Question

What is Obf (Over Braking Fault) in Altivar 71 Drive.

The fault appears when ramp adaptation is not assigned (BRA=NO), the drive is running and the DC bus voltage pass the OBF level.
Refer to attached file for more information of Obf.
Was this helpful?
What can we do to improve the information ?