Technical FAQs

Ask a Question

What is BUF (Braking Unit Fault) in Altivar 71 Drive.

This fault appears only for the drives > 90kW.
This fault appears when there is a short-circuit on the output of the braking transistor (desaturation of the braking IGBT).
Refer to attached file for more detail.
Was this helpful?
What can we do to improve the information ?