Technical FAQs

Ask a Question

Does OPC driver support Arrays or OPC DA2 (Data Access 2.0) methods.

OPC driver V1.07.00 and later supports OPC DA2 methods of connection.
You need to set the following Citect.ini parameter for this to work -
[OPC]UseOPC2=value (0=disable, 1=enable, default=0)
Citect OPC driver v1.07.03 and later supports OPC Arrays of length up to 2040 bits and also the reading of TimeStamp
and Quality data for either individual tags or whole arrays.
Was this helpful?
What can we do to improve the information ?