Technical FAQs

Ask a Question

What is the minimum system requirements for using Vijeo Citect V7.30

Processor Speed -    2 GHz
Random Access Memory(RAM) -     2GB if SCADA client Or 4GB if SCADA server.
Available Disk Space 160GB
Graphics Adapter (see note below) With 64MB of VRAM
 
Note:In Vijeo Citect it is recommended that screen resolution be set at 1024 by 768 pixels or higher.
Was this helpful?
What can we do to improve the information ?