Technical FAQs

Ask a Question

Which Operating Software we can use for Vijeo Historian V4.40.

Vijeo Historian Server & Clients can use the following Operating System :
  • Windows XP Business SP3
  • Windows Vista Business (or higher) SP2
  • Windows Server 2003 SP2
  • Windows Server 2003 R2
  • Windows 7 SP1
  • Windows Server 2008 R2
Was this helpful?
What can we do to improve the information ?