Technical FAQs

Ask a Question

What is animation points in Vijeo Citect.What is the maximum Object Animation points (ANs) per page can use in Vijeo Citect V7.20.

The points on a graphics page where an object displays. When you add an object to your page, automatically allocates
a number (AN) to the animation point, (i.e., the location of the object).
Maximum object animation that you can use on a page is 32000.
Was this helpful?
What can we do to improve the information ?