Technical FAQs

Ask a Question

What is the use of Kernel Window and how can I view the Kernel window.

If a Vijeo Citect process is running, the kernel window can be used to diagnose the runtime information for that process.
To view the kernel for a process:  
1. In Vijeo Citect Runtime Manager, right click on the process you wish to view the kernel window for.
2. Select Kernel from the context menu which appears.
3. The Kernel Window for the selected process will appear.
Was this helpful?
What can we do to improve the information ?