Technical FAQs

Ask a Question

How to make zelio smart relay SR1 applications (*.zel) compatible to zelio smart relay SR2 / SR3 (*.zm2)

 Zelio softV2.0 is available to convert program of Zelio smart relay SR1 range to Zelio smart relay SR2 / SR3
range provided the application program must be created with Zelio-soft V1.5 only
 
Option is to open *.zel application created with Zelio-soft V1.5 with Zelio-soft v2.0 and Save program as default with
type *.zel file. This saved file V2.0 (*.zel) is compatible enough to be opened with zeliosoft2 version V2.0 or onwards.
This V2.0 (*.zel) application can be downloaded to zelio smart relay SR2 / SR3. It also can be saved as zelio soft2
application (*.zm2) by save as option.
 
 
Was this helpful?
What can we do to improve the information ?