Technical FAQs

Ask a Question

When bypass contactor switch over takes place in Altistart 22 soft-starter.

When Altistart 22 starter is started, current increases and reaches to a particular peak value depending on load and then
starts decreasing. When current decreases to a value less than 120 % of Motor rated current setting (In) and motor voltage
equals line input voltage, bypass contactor is activated.
Was this helpful?
What can we do to improve the information ?