Technical FAQs

Ask a Question

What is difference between Error code E5601 and E5602 in case of Lexium 05 servo drive.

E5601 and E5602 both errors indicates missing of Sin- Cos signals feedback from motor encoder. When the drive gets no
signal at all, error 5601 will appear. When the drive gets signal is at the lower limit or partly defective, error 5602 will appear.
Was this helpful?
What can we do to improve the information ?