Technical FAQs

Ask a Question

Which range of ATS22 soft-starter suitable for inside motor winding delta type connection.

ATS22***Q range can only be used with Inside Delta type of connection from range ATS22. So, be
ensuring that ATS22***Q has been selected.
 
Was this helpful?
What can we do to improve the information ?