Technical FAQs

Ask a Question

How many PID function blocks can be used in ATV-IMC controller.

As such there is no fix figure exists regarding nos. of PID control Function blocks to be used in application.
The limitation will come from memory sixe of ATV-IMC.
ATV-IMC is available with 1 MB (Maximum) of user program size. So, it is necessary to check compiled program
size after developing an application that contains nos. of PID function blocks used.
Was this helpful?
What can we do to improve the information ?