Technical FAQs

Ask a Question

How to identify the Firmware version of EM6400/DM6200/PM1200.

There are 2 different methods to determine the firmware level in EM6400/DM6200/PM1200 meter if there is no
 communications with the meter

1-The label on the back of the meter
2-From the front panel.
Refer the attached document for the procedure;
Was this helpful?
What can we do to improve the information ?