Technical FAQs

Ask a Question

How to set the Holdup time in STBNIP2311 module.

The output of the STB Island can be maintained for a duration which can be adjusted.
To change the Holdup Time in an STB Island, go to the NIM web pages and under Configuration, select Master Controller. 
In this screen you will see an entry to change and then save this value. Typically, STBNIP2311 in a Hot Standby system,
this should be set to a minimum of 3 seconds.
Was this helpful?
What can we do to improve the information ?