Technical FAQs

Ask a Question

My Unity Pro Version V7.0 installation shows Error No 1722 with CDBSERVICES.DLL error.

It is suggested the two following actions:
 
- Manually register the dll. run "regsvr32 CDBSERVICES.DLL"
 
- If it doesn t fix the issue, uninstall the unity pro from control panel and run the attached
cleaner (to use it twice can be necessary) and then re-install Unity Pro.
Was this helpful?
What can we do to improve the information ?