Technical FAQs

Ask a Question

Is it possible to use C60 comb-busbar on DC application.

Yes, the comb-busbar for C60 range MCB can be used under DC network. And the rated insulation voltage = 500 V
 
Was this helpful?
What can we do to improve the information ?