Technical FAQs

Ask a Question

Is it possible to use the under voltage release and the shunt trip for the C60H circuit breaker at 400 Hz.

For MN under voltage release, there is a specific part number ref. 26959 for 400Hz, 115V application.
For MX shunt trip, it does not operate under 400Hz.
Was this helpful?
What can we do to improve the information ?