Technical FAQs

Ask a Question

Is it possible to use the same auxiliary contact shunt trip of C60 range with C60H RCBO.

Yes, it is possible to use the same auxiliary functions as the C60 circuit breaker, to install on the left of the C60H RCBO.
Was this helpful?
What can we do to improve the information ?