Technical FAQs

Ask a Question

Is it possible to use the auxiliary switch ref. 29450 (OF/SD/SDE) with Compact NSX DC-PV range MCCB.

 All accessories and auxiliaries of the Compact NSX DC PV breaker are identical to the Compact NSX DC range
 and it is also mentioned in the catalog.

So it is possible to use the same auxiliary switch (OF/SD/SDE) with Compact NSX DC-PV range MCCB.
Was this helpful?
What can we do to improve the information ?