Technical FAQs

Ask a Question

What is the maximum and minimum height of the bracket LA7F901 and LA7F902 used with LC1F range Contactor.

Refer below the heights of these brackets:--
 
>  LA7F901: Hmin= 51 mm / Hmax=84 mm
>  LA7F902: Hmin= 64 mm / Hmax=106 mm
Was this helpful?
What can we do to improve the information ?