Technical FAQs

Ask a Question

What are the factory default settings in DM6000 series.

The factory default settings in DM6000 series is as below,

SET Parameter
Default value
A.PRI
100
A.SEC
5.000
V.PRI
415.0
V.SEC
415.0
SYS
StAR
LAbL
123
VA.Fn
3d
bAUd
9600
Prty
Evn 1
Id
1
F.S00
100
O.F
Wh
POLE
4
Was this helpful?
What can we do to improve the information ?