Technical FAQs

Ask a Question

Will the PM1000 and PM1200 Display all three Demand Parameters (A, W & VA) simultaneously.

The PM1000 & PM1200 can read and display only one Demand (A or W or VA) Parameter at a time depending on
any one of the parameter which is selected from set up menu.

Even in Software (ION Enterprise) for the PM1200 only one demand parameter & value will be communicating depending
on the demand parameter selected physically in the meter.
Was this helpful?
What can we do to improve the information ?