Technical FAQs

Ask a Question

Do I need DISABLE the File and Printer sharing option of my PC to get ION Enterprise Web Reporter to work.

The File and Printer Sharing option must be disabled in ION Enterprise systems installed on OS .
This must be done during the install of ION Enterprise V 6.0. If this setting is not completed during the installation
process you can DISABLE the file and printer sharing option after the software has been installed, but them you must
re-install the “Report Pack” manually.
Was this helpful?
What can we do to improve the information ?