Technical FAQs

Ask a Question

For PM1000 meters, when are external CTs and/or PTs required.

External CT is required when the load current to be measured is greater than 6A.
 
An external PT is required when input voltage greater than 480V
Was this helpful?
What can we do to improve the information ?