Technical FAQs

Ask a Question

Can I restore the OLD setup parameter, while editing the Setup menu in PM1000 Series meter.

Yes, two steps are explained below.
Partially edited set up parameter: While editing the parameter if you want to restore the old set up data press the “LEFT”
key continuously up to the blinking the first digit then press the “LEFT” key once again it will resume the old setup data.
Save changes Y/N: After completing the set up table edit, when you are coming out of the set up table if “Y” is selected then
the set up will save the new changes else if “N” is selected set up will restore the values before entering the set up.
Was this helpful?
What can we do to improve the information ?