Technical FAQs

Ask a Question

What is timeout error while communicating with PM1000 & DM6000 meter and what are the reasons for this error.

When a master like EGX, ION Enterprise ,System (PC) sends a query & doesn't receive any response from the Meter 
within the wait time then the error is called Timeout Error.

Timeout errors may occur due to following reasons
      a) When meter is busy & not able to respond the query
      b) When the meter doesn't receive the entire query sent by the master or PC
      c) When there is an error in the query received by meter

Was this helpful?
What can we do to improve the information ?